2/3/2014 10:40 AM | |
Joined: 12/21/2012 Last visit: 3/9/2023 Posts: 13 Rating:
|
Hi Application-Metal Pouring in Moulding. PLC-CPU 1214C. DRIVE-YASKAWA SIGMA II SERIES SERVO DRIVE. I need technical help for servo motor controlling by PWM/PTO. In this process Controlling the metal pouringby using Joy stick (0-10v output).Servo motor connected with plunger rod.during the process operator using the joy stick for pouring plunger rod up/down and metal falling in the mould. The joy stick output voltage increased and decreased by operator. servo motor rotating Forward time plunder rod up & rotating Reverse time plunger rod down. Joy stick voltage varied according to the required flow of pouring metal. drive detail: ac I/p-3ph 230v 50hz 12A ac o/p- 0-220v 0-300hz 18.5A 2kw. motor detail: amps-16.7,watts-1800w,volt-200v,speed 1500r/min. please give solution for this servo motor control. See attached file Drive Control Diagram. Regards, G.Abi AttachmentYakawa Servo Drive.pdf (440 Downloads) |
2/3/2014 5:37 PM | |
Joined: 9/23/2005 Last visit: 7/2/2024 Posts: 4347 Rating:
|
Hi, I suggest you base your suggestion from this Application & Tools Example: SINAMICS V: Positioning of a V60 using S7-1200 (TIA-Portal) with puls/direction interface and HMI (Set 7) http://support.automation.siemens.com/BR/view/pt/38391227 |
Denilson Pegaia |
|
3/12/2018 1:06 PM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating:
|
New question published by Walter Jacquet is split to a separate thread with the subject How can the servo roll forward the entire day without any limit?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on