4/8/2014 12:04 PM | |
Posts: 2348 Rating: (263)
|
Sorry, that means you have to change CPU. Generally you can reset it by turning power on/off, but it may occur again. |
4/8/2014 2:31 PM | |
Posts: 9 Rating: (0) |
okey thank you for your help. but now it workin normaly is there any risk that will happen in the futur !! |
4/9/2014 12:23 AM | |
Joined: 8/25/2005 Last visit: 7/5/2024 Posts: 1162 Rating: (110) |
Hello mehadji, have you checked the firmware version of our CPU? The newest one at the moment should be V6.0.3 I would propose to upgrade the firmware. Detailed information could be found here: Operating System Updates: CPU412-3H / CPU414-4H / CPU414-4H PG / CPU417-4H and CPU412-5H PN/DP, CPU414-5H PN/DP, CPU416-5H PN/DP, CPU417-5H PN/DPIf you want to know something about the reason why it happend you could contact the Technical Support. You should provide the entry from the diagnostic buffer with all details and maybe your project that were load. Best regards Sabine |
This contribution was helpful to1 thankful Users |
4/10/2014 9:22 AM | |
Posts: 9 Rating: (0) |
i checked again and it's the last one V6.0.3 |
7/28/2015 1:19 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
|
Follow us on