Industry Online Support
Technical Forum
5/22/2014 3:12 PM | |
Joined: 4/20/2007 Last visit: 5/27/2024 Posts: 724 Rating: (42) |
Hi! I think you might have to download the HW including your IP for the 343 before you can use the 343.
|
5/22/2014 3:34 PM | |
Posts: 24 Rating: (1) |
i have updated and all firm ware fix same as what i have bought any idea? |
5/22/2014 3:41 PM | |
Posts: 515 Rating: (56) |
hello, also have a look at the below thread which might help you S7-1200 / STEP 7 Basic - Check list for first online access |
5/22/2014 3:41 PM | |
Posts: 24 Rating: (1) |
so what mac adress? sorry im newbie sir :( make same IP ? ip pc = ip cp343-1 lean? |
5/22/2014 3:46 PM | |
Joined: 4/20/2007 Last visit: 5/27/2024 Posts: 724 Rating: (42) |
Ip PC and ip Plc need to be same range but not the same ip. |
5/22/2014 3:47 PM | |
Joined: 11/26/2011 Last visit: 6/29/2023 Posts: 508 Rating: (22) |
MAC address is the unique address set by the manufacturer for all network devices. Amedia access control address(MAC address) is aunique identifierassigned tonetwork interfacesfor communications on the physical network segment Use PST Primary Setup tool for setting IP address to the device. Please go through the following Link to have more Idea and usage of this tool |
Last edited by: Madhava at: 5/22/2014 3:50 PM |
|
Follow us on