5/23/2014 1:46 PM | |
Joined: 4/19/2008 Last visit: 5/21/2024 Posts: 1525 Rating: (159) |
Hello Nadiya, Have a Look on the FAQ How do you implement chronological messaging with S7-400 CPUs and WinCC? Also How are message classes used if WinCC is integrated in the STEP 7 project? You have to Used the Alarm_8P Block to Gernerate the Alarm on the WinCC Side. Above FAQ Explain you the Detail Process how to do it & What you have to watch out during configuration. |
Ammy |
|
5/26/2014 8:21 AM | |
Posts: 42 Rating: (1) |
Please find the attached screen shots, I hope they are enough. I have installed AS-OS engineering and used it to automatically generate all the tags in WinCC.
AttachmentScreen shots.zip (122 Downloads) |
5/26/2014 8:22 AM | |
Posts: 42 Rating: (1) |
I'm using SFB 34 in the blocks, is that enough? |
5/26/2014 8:33 AM | |
Joined: 1/28/2009 Last visit: 5/20/2024 Posts: 6840 Rating: (1359)
|
You should try this link: How do you implement chronological messaging with S7-300 CPUs and WinCC? as you are working in S7-300 CPUs.Apparently , you are missing some steps(e.g This ). Use SFC17 or others as explained.
Update in case of an error |
Follow us on