Industry Online Support
Technical Forum
7/10/2014 11:15 AM | |
Posts: 4 Rating: (0) |
HIychervenkov, You can connect S7 200 With KTP 600 DP module with help of MPI cable. Siemens standard cable also avaliable or you can make through D connector 9 pin Type. if the you want connect S7 200 plc with KTP 600 PN ethernet type.then you need Additional Ethernet module in s7 200 side to communicate with hmi module. Regards, @JOKER |
This contribution was helpful to1 thankful Users |
7/10/2014 11:45 AM | |
Posts: 31 Rating: (0) |
Hi JOKER! Thanks. But I have a question. Do you can show links for these opportunities ? Thanks |
7/10/2014 11:52 AM | |
Joined: 9/14/2012 Last visit: 10/18/2024 Posts: 88 Rating: (14) |
Hiychervenkov, i think thislinkwill help you |
Regards, |
|
7/10/2014 12:01 PM | |
Posts: 31 Rating: (0) |
Greate. Thanks a lot. |
7/10/2014 12:34 PM | |
Posts: 5225 Rating: (1193) |
..JPEG attached.. |
7/10/2014 1:22 PM | |
Posts: 31 Rating: (0) |
Hi Wiliam! Thanks for picture. But PLC S7 CPU 226 has not a Profibus connector embedded. Thanks |
7/10/2014 1:29 PM | |
Posts: 5225 Rating: (1193) |
[smile] The connector I speak of, is a loose device. You can source them from Siemens and others. [LINK] w |
Follow us on