8/1/2014 6:20 AM | |
Joined: 12/29/2012 Last visit: 9/17/2024 Posts: 120 Rating: (15) |
Hi to All, In my Project i used S7-1200 ,CU310 PN, and 1FK7101-2AC71-1QB0 Motor With Absolute Encoder. Now i Run The Servo In MDI Mode .The operation wise Every thing Works Fine. The Problem is When Power off The Encoder Forget its Posisition. Example( Before Power Failure Encoder Posistion 100 LU After Power Failure Encoder Posistion Becomes 12000000 LU). To Avoid this Problem I enable theLoad gear, activate position tracking P2720 . But i get Only the Fault F7447. Actually this is an Absolute Encoder Why it is forgot its Posistion.Here with I attached My Starter Backup. Please Help Me to Solve this Issue Thanks in Advance....
AttachmentS120_abs.zip (294 Downloads) |
Last edited by: loga at: 8/1/2014 6:21 AMBest regards |
|
3/15/2016 11:08 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by AutoGen_226065 is split to a separate thread with the subject Absolute single turn encoder without homing. Best regards |
Follow us on