10/12/2014 11:54 AM | |
Posts: 15 Rating: (3) |
Dear MicroMan There is a difference between starting address in remote device and PDU start address which is really confusing . the startig address in PDU is one number less than starting address in remote device, I bring an example of "MODBUS APPLICATION PROTOCOL SPECIFICATION V1.1b3 " which is downloadable from www.modbus.org . I highly recommend you to study this document. it is only 50 pages. Attachmentstarting address.pdf (227 Downloads) |
This contribution was helpful to1 thankful Users |
4/14/2015 1:33 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
|
Last edited by: Min_Moderator at: 4/14/2015 1:35:43 PM |
|
5/28/2015 1:49 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
|
Follow us on