10/21/2014 11:42 AM | |
Joined: 10/11/2006 Last visit: 9/26/2024 Posts: 5907 Rating: (804) |
Hello Maged Saad, I assume that you're using a SIMOVERT Masterdrives VC. (Ending of the order no. is 6SE70..-...60). Please follow the compendium section 6.3 detailed parameterization => Drive settings and carry out the automatic parameterization. The motor can be set via code no which is given in the compendium also "List of stored motors" It seems that the motor has the no. 25. no. 25; 1PH7184-2_F_; 1750rpm; f=59.0Hz; I= 120.0A; U=388V; Torque=327Nm; cos_phi=0.780; Iu=52.9A The link to the compendium Masterdrives VC 3.4: http://support.automation.siemens.com/WW/view/en/13472409 While coming on a existing machine the following sections are of interest or important: 5.5 Handling DriveMonitor 6.3 Detailed parameterization 6.4 Hints for parameterize 7.2.8 Functions for automatically motor parameterization and -identification 8.2 Profibus communication function diagrams Basic functions (The best is printing them out) |
With best regards, |
|
Follow us on