11/19/2014 11:21 AM | |
Joined: 4/24/2006 Last visit: 9/10/2024 Posts: 8736 Rating:
|
Hello, Try to perform an OS update, with the option "Reset to factory settings" Best regards, Wizard |
11/19/2014 1:43 PM | |
Joined: 4/24/2006 Last visit: 9/10/2024 Posts: 8736 Rating:
|
Hello, Please have a look at the following link: how do you do an "Operating system update" (OS update) or "Reset to factory settings" on operator panels? Best regards, Wizard |
11/19/2014 2:36 PM | |
Posts: 5 Rating:
|
Thak you very much I'll check this Regards Ahmed |
11/20/2014 3:25 PM | |
Joined: 4/24/2006 Last visit: 9/10/2024 Posts: 8736 Rating:
|
Hello, Have a look at the following link: Which connector cables are available for connecting to SIMATIC Panels? (The option 'reset to factory settings' is only possible when you use Ethernet Perhaps you should try using Prosave. fill in the IP address of the panel and the MAC Address. Then push button "OS update". Now you should boot the panel (Power up) Best regards, Wizard |
This contribution was helpful to
1 thankful Users |
Follow us on