11/22/2014 9:32 AM | |
Joined: 5/28/2014 Last visit: 12/31/2023 Posts: 32 Rating:
|
i am using WinCC V7.2 ... and i cannot find the functon GetCursorPos () in it. |
11/23/2014 11:58 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating:
|
Hello typedat, the function "GetCursorPos()" is no WinCC-function, it belongs to the Windows-OS. see: http://msdn.microsoft.com/library/windows/desktop/ms648390(v=vs.85).aspx To use it in a C-script in WinCC, you have to declare Windows.h and user32.dll. Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
11/26/2014 7:43 AM | |
Joined: 10/3/2010 Last visit: 7/5/2024 Posts: 1556 Rating:
|
If you use VBScript on event Mouse Press Left, Release Left, ... you already get the coördinates where you clicked by default: Sub OnLButtonDown(ByVal Item, ByVal Flags, ByVal x, ByVal y) ... End Sub there you can use x & y as a starting point to position your popup |
B r g d s , |
|
This contribution was helpful to
2 thankful Users |
7/7/2017 10:58 AM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating:
|
New question published by JLTwardy is split to a separate thread with the subject Windows in "C' Script Winncc - Example?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on