1/3/2015 5:11 AM | |
Posts: 30 Rating: (2) |
Hello, EDIT ON 26/09/2018 Hi, When you guys set up Remote PLC Gateway (2.1.Setup of remote PLC), be careful because that IP is the one you set in Ethernet Properties - TCP/IPv4. If you do in a wrong way, you couldn't connect to your remote devices (PLC, HMI, etc,...).Best Regards, AttachmentHow to setup Teamviewer VPN.pdf (6701 Downloads) |
Last edited by: MinhPhong29 at: 9/26/2018 10:43:37 AMLast edited by: MinhPhong29 at: 9/26/2018 10:43:58 AMLast edited by: MinhPhong29 at: 9/26/2018 10:54:37 AM |
|
This contribution was helpful to6 thankful Users |
1/3/2015 9:47 AM | |
Posts: 30 Rating: (2) |
Hello ChristophD, I did step by step as the attachment. I have added route to the PLC on the PG, but I can't find accessible nodes. |
6/19/2015 9:20 AM | |
Joined: 8/11/2011 Last visit: 11/27/2023 Posts: 51 Rating: (1) |
Hi, I can ping the remote Laptop via VPN, Thanks. |
Follow us on