1/30/2015 9:48 PM | |
Posts: 311 Rating: (3) |
Hello all, I can not find the HW support package for the module 6ES7 241-1CH32-0XB0., I'm using TIA V12 SP1 Update 4. Regards Per Olof |
1/30/2015 10:51 PM | |
Posts: 311 Rating: (3) |
Hello, Yes, I have locked inside this support package but is not there: |
1/30/2015 11:07 PM | |
Posts: 311 Rating: (3) |
I have V12 SP1 Update 4 installed, but the module is not within the cataloge, see picture. |
1/31/2015 8:51 AM | |
Posts: 311 Rating: (3) |
Anyone that got any ideas ? Does V13 got this moudle in the HW cataloge ? |
1/31/2015 10:31 AM | |
Posts: 784 Rating: (52) |
Yes,you can get this module inTIA HW catalogue V13
|
1/31/2015 11:21 AM | |
Posts: 311 Rating: (3) |
Anyone that got this module in TIA V12 ? |
Last edited by: Per Olof at: 2/2/2015 11:52 AM |
|
2/2/2015 12:30 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715) |
Hello,
In short, you can configure the older module and insert the new one, the module should work but only without any new features. |
Problem solved? |
|
Follow us on