(0)| 2/5/2015 6:39 PM | |
|
Posts: 17 Rating:
|
Hello everyone, i am having two station of S7-400H system, two server (one as main server and other one as stand by) and three client. The system was working before. Now i am changing the CPU of main server with new CPU. so i have installed two CP card from the old CPU to new one. CPU is having Windows XP service pack-2. I have installed wincc explorer version 6.2 + sp2 and SIMATIC NET for industry network. But i ma not able to see any of CP card in Network area of computer. I can see it under SIMATIC NET in device manager. I am not able to set up communication with PLC due to this problem. I am not able to find NDIS adapter for CP card anywhere in my computer or while the installation of SIMATIC NET. Please help me.
-------------------- Splitted from Configuring Windows Network using CP1613/23 |
Last edited by: Min_Moderator at: 2/6/2015 11:31:56 AMNew subject after splitting |
|
Follow us on