3/4/2015 10:24 AM | |
Posts: 5225 Rating: (1193) |
Andrew - while you wait for an expert's opinion, here is my opinion.. Do you have a licensed version of STEP7 V5.5 installed on the computer where you are trying to make the converting process with TIA12? Please check what are all the requirements you need to convert a PLC program. Also.. Consider that you do not have to convert the PLC program to make a HMI program.There are 3 options.. 1. If you already have an old HMI program (not too old), you can have TIA12 migrate the HMI project. 2. You can reduce the STEP V5.5 to only a shell of a program.. only having the DBs and M-flags that you need to link to the HMI. 3. Make a loose standing HMI project. You have to type in all the variables and create the link to the PLC using a manual process. If you need help in creating a new HMI project when you do not have the PLC program in the same project.. than please try the Product Conferences > Visualization > SIMATIC WinCC (TIA Portal) conference. Helpful? |
Last edited by: William B. at: 3/4/2015 10:25:28 AM@Christoph: did not see your post.. no disrespect intended. |
|
3/4/2015 6:18 PM | |
Joined: 5/12/2006 Last visit: 10/15/2024 Posts: 22414 Rating: (3017) |
Hello,
yes this is possible. for further Information to this usecase lokk here: |
This contribution was helpful to1 thankful Users |
3/4/2015 6:23 PM | |
Posts: 5225 Rating: (1193) |
Surely THAT is the solution that is going to be the best.
|
Last edited by: William B. at: 3/4/2015 6:26:26 PM |
|
Follow us on