(1)| 3/5/2015 5:08 PM | |
|
Posts: 1 Rating:
|
Dear Expert Do you have a project sample(s) for programming analog input Volt and Current (S7-1200) as well?? where to down load them from? Regards,
-------------- |
Last edited by: Min_Moderator at: 3/6/2015 9:21:41 AMNew subject after splitting |
|
| 3/5/2015 5:24 PM | |
|
Posts: 5225 Rating:
|
Handling [0 .. 10] V or [0 .. 20] mA looks the same if the hardware is capable to measure these. The trouble comes in when handling [4 .. 20] mA on hardware that is set for handling [0 .. 20] mA. Please have a look at... [LINK] w |
| 3/6/2015 10:23 AM | |
|
Posts: 1058 Rating:
|
Hello LionPLC, look here for an example: Process Data Acquisition and Monitoring with SIMATIC S7-1200 regards |
Follow us on