3/28/2015 12:57 AM | |
Posts: 5 Rating: (0) |
hi I am making s5 to s7 conversion now and I found the error after the conversion. the error is in OB1 exactly by calling PB13 PB15 and PB22 and _ PB23 .these are found also found in the list of PB blocks in the s5 programe .but they are called in OB1 s5. So why they are called in OB1 despite PB 13, PB15, PB 22, PB 23 are not present in PB programe S5 Best Regards
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 3/30/2015 3:52:02 PMNew subject after splitting |
|
3/28/2015 11:51 AM | |
Posts: 5 Rating: (0) |
hallo but i don't understand in the programe why the OB1 call PB 13, PB15, PB 22, PB 23 and this bloc they not existe in PB .here you will find the S5 program and and the program converted s7 with error: AttachmentSOUTIREUSE S5 (1).rar (169 Downloads) |
3/28/2015 11:55 AM | |
Posts: 5 Rating: (0) |
and this the programe converted to s7 WITH ERRORE: THANK YOU AttachmentWAJ.rar (184 Downloads) |
3/29/2015 11:34 AM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating: (131) |
Hello, now i understand your problem. Please check if offline and online is the same. Maybe there are differences and the blocks are only in the PLC or the PLC runs with error. Regards André Räppel --------------------------------------------------------------------------------- www.raeppel.de
work faster with innovative PLC-Tools |
Follow us on