4/2/2015 11:26 AM | |
Joined: 2/6/2015 Last visit: 9/21/2017 Posts: 38 Rating: (1) |
Hi All, I am new to Siemens as well as to the field of communication. I have some questions regarding the communication between any ERP and the siemens HMI/PLC. 1. What is the best way and what are the possible ways to get the manufacturing data from ERP using HMI/PLC and communicate it to the individual machines in a plant ? and also to collect the information from the machines and communicate it back to the ERP? 2. In my case it is S71500 type PLC connected with TP1500 comfort panel, which acts as a master. This master should get data from ERP and communicate it to the individual machines' PLC. 3.I did some research and came across this product (devicewise) and again it says its available only for S7300 type of PLCs. 4. Simatic IT Production Suite ? Any input would be of great help. Thanks and Regards, |
Last edited by: dawson_1985 at: 4/2/2015 11:33:59 AM |
|
1/5/2016 4:45 PM | |
Posts: 2 Rating: (0) |
Hello , Did you find any solution for how to connect PLC to ERP ? |
Follow us on