4/7/2015 9:47 AM | ||
Posts: 3 Rating: (0) |
Thank you for the advise. Item 1 &2 error did not show up anymore. However, I still encounter error of item 3&4 : Module IM 153-2 OD cannot migrated. Is there any other step I can take?
|
|
4/7/2015 10:03 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981) |
Hello,
which modules you have placed behind the ET200 Interface module? Can you export the HW Config of the classic project to a cfg File and post it here, please.
Christoph |
4/7/2015 10:25 AM | |
Posts: 3 Rating: (0) |
Hi, Please refer attachment, I try to paste here but too many line.
Attachmentplc1.zip (154 Downloads) |
Last edited by: stephnsl at: 4/7/2015 10:39:08 AM |
|
4/7/2015 10:38 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981) |
Hi,
it looks that this station is not configured with Step7 only. The ET200M is configured with PDM Software (PCS7), an this components are not supported in TIA. Regards CHristoph |
Last edited by: ChristophD at: 4/7/2015 11:21:06 AM |
|
This contribution was helpful to1 thankful Users |
10/15/2017 7:40 PM | |
Posts: 1 Rating: (0) |
hi i ask when i make migration to v13 the errors appears like in the figure. i asked portal v13 did not support all this is IM medule |
10/16/2017 9:08 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
correct the modules are to old, and not supported in tia. |
Follow us on