4/16/2015 9:23 AM | |
Joined: 10/17/2011 Last visit: 7/19/2022 Posts: 148 Rating:
|
Dear Experts, I have installed PCS7 V8.0 SP1 on my laptop with Windows 7 as an OS. i am facing problem with WinCC, when I create new project in winCC or add OS station in PCS7 project, I am not able to create it, if LAN is not connected.I get error "Unspecified Error" and Project get closed. If I connect LAN connection and try, then everything works fine. How to resolve it? Please suggest. By connecting LAN , does any service starts which is necessary for creation of WinCC project? Warm regards, Damayanti Bhapkar -------------- |
Last edited by: CS Moderator at: 4/16/2015 1:16:33 PMnew subject after splitting |
|
4/19/2015 7:42 AM | |
Joined: 10/17/2011 Last visit: 7/19/2022 Posts: 148 Rating:
|
Dear, I tried by assigning valid IP address, still problem not resolved. Anything else can we try? Damayanti |
4/20/2015 8:53 AM | |
Posts: 567 Rating:
|
Hi Damayanti,
thanks for feedback. I know the issue and I have solved it with a valid IP. So there must be another reason for the issue Maybe there some other settings not correct. Did you check your network settings? They should be as described in PCS 7 Compendium Part A chapter 3.3.5. Link: https://support.industry.siemens.com/cs/ww/en/view/107196780/72204301323 Especially the hints are very usefully. |
Follow us on