(0)| 4/22/2015 7:02 AM | |
|
Joined: 10/12/2014 Last visit: 3/17/2025 Posts: 66 Rating:
|
My hardware configuration is one 115 u cpu get I/O from 2 remote stations(ET 100U Distributed I/Os ) . This 2 remote stations (ET 100u) connect with separate 2 serial links via 308-3UA12 Expansion Unit Interface Module . my fault is I can not operate these 2 et 100 u stations simultaneously .At one time this can operate only one.This means i stop one manually by ON/OFF switch ,then other station can ON.Then i ON the off station,there blink I/O disable bulb in red. Here I attach i stack and B stack and hardware configuration. AttachmentATTCHMENET22042015.zip (774 Downloads) |
Last edited by: neththi at: 4/23/2015 5:23:42 AM |
|
| 4/23/2015 5:24 AM | |
|
Joined: 10/12/2014 Last visit: 3/17/2025 Posts: 66 Rating:
|
Communication error with 308-3UA12 Expansion Unit Interface Module and ET100u SIR ; My hardware configuration is one 115 cpu u get I / O from 2 remote stations (ET 100 Distributed I / Os). This 2 remote stations (ET 100u) connect with separate 2 serial links via 308-3UA12 Expansion Unit Interface Module. my fault IS I can not operate 2 et100 u stations Simultaneously .At one time this can operate only one.This Means i stop one manually by ON / OFF switch, then other station can ON.Then i ON the station OTHER off station there flashing I / O disable bulb in red. Here I attach i stack and B stack and hardware configuration . My understanding figure is erase eprom program on 308-3UA12 Expansion Unit Interface Module .Can it happen ..???sir .. Can u send me sir COM ET 100 communication software ??? I cant find this software from internet. AttachmentATTCHMENET22042015.zip (813 Downloads) |
Last edited by: neththi at: 4/23/2015 7:59:29 AM |
|
Follow us on