5/9/2015 8:55 PM | |
Posts: 1 Rating:
|
Hi All,
Does anyone know if I can purchase a USB Device so I can write directly from my PC running Portal Version 13 to a Siemens SD card? I would like to be able to load an SD Card at the office from my PC and Take the Card to the Site, install it in the PLC start and Run. If you can help with a P/N I would be very grateful. Thanks, Kevin Williamson
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 5/11/2015 11:37:58 AMNew subject after splitting |
|
8/20/2019 11:48 PM | |
Posts: 1 Rating:
|
Hello, is there any procedure to do it or a special SD configuration? Do I have to change the SD card after the program transfer? Thanks for information |
Follow us on