5/13/2015 2:45 PM | |
Joined: 7/23/2014 Last visit: 1/17/2020 Posts: 1 Rating: (0) |
Hello, do you have any example about that? So, I try to explain what I want to do: I have aCPU 1212C with 1241 module. I want to read two analog input (0/10V) and i want to send the two values at two diferent slave panel meter with modbus rtu communication. I have created part of the program, but how i can send the values at the same time (automaticly) Can you help me? My "siemens level" is very very low ... Thank you very much!!
---------------------------------------------------------------------------------------------------- AttachmentRTU16_PROCESOS_R10.rar (113 Downloads) |
Last edited by: pedroso at: 5/13/2015 2:46:17 PMLast edited by: Min_Moderator at: 5/13/2015 5:15:19 PMNew subject after splitting |
|
Follow us on