5/18/2015 5:52 PM | |
Joined: 11/12/2014 Last visit: 10/31/2023 Posts: 11 Rating: (2) |
hello experts. I'm with a big problem. I have a flying cutting machine, cutting measures vary widely. WHAT know can not be, do you guys mind? The screw is configured correctly, the timing is perfect with the material. I have used the S7-1200 and Yaskawa servo motor. ----------------------------------------------------------------------------------------------------
Split from S7-1200 and servo controlled "flying saw" problems. |
Last edited by: Min_Moderator at: 5/19/2015 8:56:12 AMNew subject after splitting Douglas Silva |
|
5/18/2015 10:09 PM | |
Joined: 11/12/2014 Last visit: 10/31/2023 Posts: 11 Rating: (2) |
I'm using a pulse train control for the Yaskawa servo motor. My strategy is: 1) Yaskawa servo motor control via PTO 2) Use the HSC to measure the linear speed cutting and 3) Use "Move Velocity" block to make the cut The variation is independent of speed, both low (200mm / s) and for high (500mm / s) does not exist an error pattern. The first pieces are cut within a range of 1-2mm. hardware: * S7-1200 Firmware 3.0 Step7: * Tia Portal V13SP1 Annex the project. AttachmentAnanda0405V03.rar (507 Downloads) |
Last edited by: DougPin at: 5/18/2015 10:14:17 PMLast edited by: DougPin at: 5/18/2015 10:14:43 PMDouglas Silva |
|
9/28/2017 1:11 PM | |
Joined: 6/19/2017 Last visit: 8/5/2024 Posts: 8175 Rating: (169) |
New question published by Vo Trong Nguyen is split to a separate thread with the subject How to syncronized the shear and material ( both cutting position and speed to get the length exactly)?. Best regards |
My Forum is the place to personalize your profile, |
|
8/9/2024 8:09 PM | |
Joined: 2/12/2024 Last visit: 8/9/2024 Posts: 1 Rating: (0) |
hi, did you solve it? |
Follow us on