5/19/2015 4:51 AM | |
Posts: 1 Rating: (0) |
Buenas Noches estoy comenzando a trabajar con el TIA Portal V13, y tengo la tarjeta SM331 AI 2x12Bit (331-7KB01-0AB0), y no la encuentro, puedo actualizar el Catalogo? o me resigno a que no podre utilizarla con el TIA Portal V13? Good Night, i begin to work with TIA PORTAL V13, and i have the card SM331 AI 2x12Bit (331-7KB01-0AB0), and i can´t find it in catalog, can i update the catalog? thanks for answer my question. Ing. Edgar Maya Pérez. Teacher of IPN, México.
---------------------------------------------------------------------------------------------------- |
Last edited by: AutoGen_1055330 at: 5/19/2015 4:53:08 AMLast edited by: Min_Moderator at: 5/19/2015 1:56:51 PMNew subject after splitting |
|
5/19/2015 5:50 PM | |
Posts: 5225 Rating: (1186) |
Hi. Friend Christoph has already answered the heart of the question. Step7 V1x (as component of TIA Portal) can also handle the newer range PLCs: S7-1200 and S7-1500, and then newer versions of PLC hardware associated with the S7-300 and S7-400 family of PLCs. If it is for your own use - see if you can dust off an older Step7 V5.x version that was used with the hardware you have. If it is for your students - I would recommend you get hold of the S7-1200 family. Under TIA Portal V13 SP1 it is now possible to simulate the S7-1200 PLC. It may be worth your while.. do get hold of the Siemens guys guys near you and chat to them about how they can help you. Greetings. |
This contribution was helpful to1 thankful Users |
4/25/2017 11:20 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by fiah is split to a separate thread with the subject SM331 with TIA V13. Best regards |
Follow us on