(0)| 6/3/2015 3:50 PM | |
|
Posts: 1 Rating:
|
I am having a similar problem with the migration. I am able to migrate, and have fixed the HMI tags and text lists with no issues. After trying to compile the project to download, I get errors for the "Animation Appearance in various screens saying there are invalid parameters". I have checked for the correct addressing that is being used in the original project, all seem to be correct. These errors are also, showing up in my scroll lists.
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 6/8/2015 10:27:31 AMNew subject after splitting |
|
| 6/12/2015 7:14 AM | |
|
Posts: 1299 Rating:
|
Hello, if you click on the arrow in column "Go To" next to the error text you can see the objects which are causing the problems. K!ke |
Follow us on