11/19/2009 3:28 PM | |
Joined: 3/6/2009 Last visit: 4/3/2024 Posts: 2 Rating:
|
Wizardthank u very much . it's worked |
12/2/2009 9:48 AM | |
Joined: 4/24/2006 Last visit: 6/28/2024 Posts: 8698 Rating:
|
Dear Ayman Elotaify, Sorry, but I think the following explanation is the only correct one: When you use the buttons ESC + Cursor Right + Cursor Down and at the same time switch on the Power, you will go to Transfer mode, but also delete the project on panel When you use the buttons ESC + Cursor UP and at the same time switch on the power, you will go to Transfer mode and the project will stay on the panel So you can use Prosave to back up project. Please have a look in manual: OP7, OP17 Operator Panel See chapter 3.1 (page 3-5) Best regards, Wizard |
This contribution was helpful to
2 thankful Users |
12/1/2011 4:56 PM | |
Posts: 7 Rating:
|
I can not do it |
Last edited by: Cantu at: 12/1/2011 5:01 PM |
|
Follow us on