(0)| 7/19/2015 1:38 PM | |
|
Posts: 1 Rating:
|
i am using converter 6SE7027-2ED61-Z. i have problem now a days that drive is showing current about 20 A but the motor is not moving a bit and drive is in ON state always and not showing any Fault. I am using 30 kw siemens motor 1LG4 223 - 6AA90 - Z. i have changed whole drive 3 times. i have changed the motor & it's incremental Encoder also. i have checked all Earthing, all is ok. all hard wiring but not succeeded to find the problem?? what i should do now?? ---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/20/2015 3:07:37 PMNew subject after splitting |
|
| 9/11/2015 3:27 PM | |
|
Posts: 29 Rating:
|
Change the phase sequence of motor in the terminal box of the motor and check whether encoder give +ve pulse if u give clockwise direction...... |
| 11/11/2015 10:11 AM | |
|
Posts: 93 Rating:
|
friend can u try download the original paramter to the inverter |
Follow us on