7/23/2015 7:03 AM | |
Posts: 15 Rating: (0) |
Dear Mr/Mrs KSN I have problem with upload Program Simadyn D I don't know when I upload program and can I used software Step7 Manager? Now, I have some project since 2001, format *.USP and how I can read it. I don't know software. Please, can you help me? Thanks you very much!
---------------------------------------------------------------------------------------------------- |
Last edited by: khanhmydhd at: 7/23/2015 7:21:07 AMLast edited by: Min_Moderator at: 7/23/2015 3:34:50 PMNew subject after splitting |
|
7/23/2015 7:14 AM | |
Joined: 8/25/2006 Last visit: 7/17/2024 Posts: 2207 Rating: (278) |
Hello. May be you have *.UFP files? |
This contribution was helpful to1 thankful Users |
7/23/2015 7:18 AM | |
Posts: 15 Rating: (0) |
Dear Mr/Mrs KSN! Yes! I already mistake. Exactly *.UFP Can you help me? |
7/23/2015 7:38 AM | |
Joined: 8/25/2006 Last visit: 7/17/2024 Posts: 2207 Rating: (278) |
These files are made using STRUC. UFP - uncompiled function packet, UMP - uncompiled Master program. Simatic Manager can not be used to read these files. If you just want to see the code, you can use Strucview program. To be able to edit and comile you will need STRUC. |
This contribution was helpful to1 thankful Users |
7/23/2015 8:35 AM | |
Posts: 15 Rating: (0) |
Thank you very much! I already read program *.UFP. But I can't modify it. I don't find tool STRUC.UFP. And now, can I connect from PC to simadyn D with software Step7 Manager and upload program ?. Because with Step 7 + CFC + D7 SYS, i see it can created new project with SIMADYN D Station B.R |
Follow us on