(0)| 8/6/2015 12:05 PM | |
|
Posts: 5 Rating:
|
We have use to S7-300 (315-2DP) CPU and IM module ET 200 with DI-8Ch module- 3 no's DO-16ch-module-1 no's,AI-8ch module-1 no's,AO-8ch-1 no's ET-200- 6ES71532BA020XAB0 DI-6ES73211BH020AA0 DO-6ES73221BH010AA0 AI-6ES73311KF020AB0 AO-6ES733125HF000AB0 We need each IO module health bit status & Fault bit status .so how we can get the IO module status health bit (Health bit mean the particular module working good or fault). Please give me a best solution. We are using ladder logic .so please give me a best solution how is call to health bit status and fault bit status. We are waiting your valuable feedback ---------------------------------------------------------------------------------------------------- Split from PLC/DCS Monitoring Closed cause question posted twice. The second thread with the subject Module status for health bit and fault bit is published within the conference SIMATIC S7-300 / S7-300F. |
Last edited by: CS Moderator at: 8/6/2015 3:02:56 PMNew subject after splitting |
|
Follow us on