8/6/2015 1:00 PM | |
Posts: 4 Rating: (0) |
GOOD DAY ALL WE HAVE THE SAME ISSUE ON TP 177B. THE POWER IS OK BUT THE BACK LIGHT IS SHOT. THE CLIENT DOES HAVE A SPARE UNIT IN STORES. OUR PROBLEM IS THE CLIENT DOES NOT HAVE THE SOURCE CODE FOR THIS PROJECT. IS THERE ANY WAY TO BACKUP OR MAKE A COPY OF THE SOFTWARE FOR THE TP 177B?? THANKS GUYS!
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/13/2015 2:03:58 PMNew subject after splitting |
|
8/6/2015 4:42 PM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hello NAZEER_RSA, If you are lucky that the panel has enabled the option "Enable Backtransfer" should work with Prosave Have a look at what you need for your panel: How do you backup/restore with a Windows-based panel? What transfer options are available in the various operator panels? |
Follow us on