8/27/2015 2:47 PM | |
Joined: 5/7/2015 Last visit: 9/20/2023 Posts: 56 Rating:
|
Hi Denilson, Thanks a million for the wonderful example and docucmentation. It works well even when modified considerably. I have 3 slaves and these were polled at a rate of 100 ms. with zero error.
However now, I need help in moving this block to another project. So I moved the Master_Modbus FB 775 to a new library and from that library, I moved this to the main project . When I compile it gives errors all pertaining to the control states such as Tag "INIT" not defined, Tag "Config_modbus" not defined, Tag "Data_Transfer" not defined. Please help me to fix these. If I am not mistaken - I am not an expert in SCL- these are values assigned to the Integer parameter #Control.state. This aspect I have not understood. This problem apart, I appreciate your help in guiding us all. regards ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/27/2015 3:56:19 PMNew subject after splitting |
|
Follow us on