8/31/2015 3:33 PM | |
Posts: 5225 Rating: (1189) |
okay... Let us take this to the next level. 1. Unzip the attached file - You will get LowPassFilter.scl. 2. Add the source to a project by selecting "add new external file". Use a new project - just to be on the safe side. 3. Right click the SCL file and ask for "generate blocks from source". 4. A new FB will be created with SCL code inside. w AttachmentLowPassFilter.zip (331 Downloads) |
Last edited by: William_B at: 8/31/2015 8:00:24 PMreplace source file |
|
8/31/2015 5:45 PM | |
Posts: 5225 Rating: (1189) |
Sorry about the error... in haste I changed the author name from my work-alias to the forum-alias without thinking of the typing rules they apply. The SCL source was replaced in the earlier post. [Normalized] This is not a rule. The function works without regard to the 0.0 - 1.0 range.
Definition of "Influence" - contribution / weight / value added With #Factor := 0.1 the now input reading will contribute 10% to the output while the previous result (history) will contribute (100% - 10%) 90% to the output .
Does this help you? |
Last edited by: William_B at: 8/31/2015 8:08:51 PMnew information; text in italics Last edited by: William_B at: 9/1/2015 10:21:38 AMDefine what "influence" means to me. Rewrite paragraph for clarity. |
|
Follow us on