9/17/2015 6:05 AM | |
Posts: 3 Rating:
|
Hello, I request an English language version of the following two documents: (a) https://cache.industry.siemens.com/dl/files/932/8790932/att_82256/v1/norm_tab.pdf (b) https://cache.industry.siemens.com/dl/files/748/109476748/att_845617/v1/IEC_61131_compliance_de_DE.pdf Further, I request further information (in English) on the subject of: (a) why Step 7 is not in full compliance with IEC 61131-3: 2013 (see Tables 48 to 53 in this standard) and (b) what is Siemen's policy is towards full compliance with IEC 61131-3: 2013. Thank you. ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 9/17/2015 11:58:56 AMNew subject after splitting |
|
9/17/2015 7:10 AM | |
Joined: 1/28/2009 Last visit: 8/26/2024 Posts: 6846 Rating:
|
Hello, I request an English language version of the following two documents: (a) https://cache.industry.siemens.com/dl/files/932/8790932/att_82256/v1/norm_tab.pdf (b) https://cache.industry.siemens.com/dl/files/748/109476748/att_845617/v1/IEC_61131_compliance_de_DE.pdf I think you are looking for the following links in English: General Product Approval, Manufacturer declartion, ManufacturerI hope this helps, hdhosseini |
This contribution was helpful to
2 thankful Users |
9/17/2015 12:01 PM | |
Joined: 9/1/2005 Last visit: 8/12/2024 Posts: 4104 Rating:
|
closed cause question published twice.
The second thread with the subject STEP-7 -- IEC61131-3 Certification is published within the same conference.
Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on