9/28/2015 2:43 PM | |
Posts: 5225 Rating: (1193) |
Hi. Today in my email inbox was the FAQ from Siemens: Having not used my simulation package this month I investigated and found that I need to follow the FAQ. I proceeded doing the installation of Update 1 for PLCSIM V13 SP1. This action however did not resolve the issue. The messages that come up after installing the update: My PC then is "unusable", making clicking sounds when moving the mouse. It takes keyboard commands to shut down the effected systems. The installed version seems to be okay however: The installation was done.. My PC system: ----- w |
Last edited by: William_B at: 9/28/2015 2:51:16 PMadd info |
|
9/28/2015 2:57 PM | |
Posts: 8946 Rating: (999) |
What AV you are using... If AVG, please read here (if not already done..) https://support.industry.siemens.com/cs/ww/en/view/109479615 |
9/28/2015 3:02 PM | |
Posts: 5225 Rating: (1193) |
Thank you for the warning.. I am aware of this issue (even if not an AVG user). Several of Siemens' software has false positive issues (example: MicroWin). I doubt this is the issue though - I had the AV continuously disabled while doing the installation & for starting up the software for first use. |
Last edited by: William_B at: 9/28/2015 3:03:30 PM |
|
9/29/2015 9:25 AM | |
Posts: 8946 Rating: (999) |
This morning, Upd. 5 for V13SP1 is announced: https://support.industry.siemens.com/cs/ww/en/view/109311724 https://support.industry.siemens.com/cs/ww/en/view/109439573 Again some GB of bugfixes (and perhaps new bugs?) There is til now no update für PLCSIM, but worth a try... |
This contribution was helpful to2 thankful Users |
9/29/2015 9:43 AM | |
Posts: 5225 Rating: (1193) |
A very good suggestion. Thank you. When in the middle of a project Remember Update 5 for TIA13 SP0?.... |
9/29/2015 9:51 AM | |
Posts: 8946 Rating: (999) |
Therefor, always ever ever do a complete Image before install new Simatic Software. By high frequency of TIA Updates that means, Image every day.... Anyhow, I wish good look and hope it solve your problem! |
This contribution was helpful to2 thankful Users |
Follow us on