10/2/2015 3:53 PM | |
Posts: 68 Rating: (0) |
I have SCALANCE XB008 UNMANAGED INDUSTRIAL ETHERNET SWITCH. I add new device to PRFInet IO and I set IP. I download configuration to S7-300. When I open modul information and I open interface I see that IP is 0.0.0.0 and I have Error LED (SF) Error LED (BUS2F). How I can set the IP in my situation. AttachmentScreenshots.zip (177 Downloads) |
Last edited by: Min_Moderator at: 10/5/2015 10:18:38 AMAdd attachment |
|
10/2/2015 7:32 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (307) |
Hello, First, The XB008 has nothing to do with your problem.
See a comparable example here in annex. You do that for each device. An be sure that the device names are unique over the complete network.
AttachmentStep7 classic - IO device - Assign device name.pdf (151 Downloads) |
Last edited by: jklm at: 10/2/2015 7:33:37 PMLast edited by: jklm at: 10/2/2015 7:39:23 PMBest regards |
|
10/3/2015 12:35 PM | |
Posts: 68 Rating: (0) |
Yes, I have ethernet inteface and my set PG interface are OK. couse I can go to ONLINE in HWconfig and I can download program to device. |
10/3/2015 5:08 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (307) |
Hello, And of course, you must be connected on the network where the device is connected. An alternative way to set a name (among other functions), is the free tool PRONETA. |
Best regards |
|
This contribution was helpful to1 thankful Users |
Follow us on