10/16/2015 9:40 PM | |
Joined: 3/14/2015 Last visit: 10/29/2023 Posts: 93 Rating: (0) |
I Have somehow the same problem. One 416-3dp with IF 964-dp in a project should be connected to a 315-2dp via 342-5 in another project. What is the configuration? Master-master or master-slave? Should I used "unspecified" for connection partner in netpro? Which functions I need to use on both sides? (S400 side is pcs7) I really need it ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/19/2015 2:53:44 PMNew subject after splitting |
|
10/17/2015 10:33 AM | |
Joined: 3/14/2015 Last visit: 10/29/2023 Posts: 93 Rating: (0) |
Consider that 416 and 315 are NOT in the same project! |
Last edited by: Hasan1987 at: 10/17/2015 11:07:12 AM |
|
Follow us on