10/19/2015 9:15 PM | |
Posts: 3 Rating: (0) |
Hi ........................... prosave can not connecte to mp370 The bootloader starts, but then nothing black screen |
10/21/2015 9:29 AM | |
Joined: 4/24/2006 Last visit: 9/19/2024 Posts: 8739 Rating: (1168)
|
Hello chifra, It is possible with the cable used, to perform an OS update, see the following link: Which connector cables are available for connecting to SIMATIC Panels? Try to perform an OS update with the option "Reset to factory settings" selected, see the following link: Best regards, Wizard |
This contribution was helpful to1 thankful Users |
Follow us on