11/6/2015 2:20 PM | |
Joined: 5/9/2015 Last visit: 7/25/2024 Posts: 81 Rating: (4) |
Hello, I am using PCS7 V 8.1 and using hart modules with redundant controller (CPU410-5H) i have prepared the configuration for AI, AO, DI, DO modules. Except AI for all other modules the channel driver are generated without any issue. AI & AO are HART modules. I am not able to generate the channel driver for the analog input modules even i have connected the Hart field devices as well in the channels as shown in the attachment. Can you please suggest what could be the reason for that. Best regards, Naresh Saini ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/9/2015 10:51:15 AMNew subject after splitting |
|
6/24/2020 11:00 PM | |
Posts: 23 Rating: (0) |
Need to activate ticks in Diagnostics filder for required channels |
Follow us on