11/20/2015 5:09 AM | |
Joined: 11/25/2009 Last visit: 5/5/2024 Posts: 33 Rating: (0) |
Hi DCHARTIER, I was searching through the forum regarding my problem and ultimately found this thread, my problem is the reverse process means to convert the WinAC program either S7-400 or S7-300 is it possible? If so than please help me I would be grateful to you. Regards.
------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/20/2015 11:26:29 AMNew subject after splitting |
|
12/3/2015 3:09 AM | |
Joined: 9/27/2006 Last visit: 7/4/2024 Posts: 12267 Rating: (2675) |
Hello venom; Is the missing connection to the ACROPOVIS station (# 21) in your Netpro screencapture? If so it would seem you need to recreate the connection manually. If you have little experience doing this operation, please read the section on Connections in the following manual: CPU-CPU communication with SIMATIC controllers (compendium) https://support.industry.siemens.com/cs/ww/en/view/20982954 Hope this helps, Daniel Chartier
|
Follow us on