(1)| 10/2/2015 3:38 PM | |
|
Posts: 4 Rating:
|
Dear Expert I have a problem with TP700 comfort & s71200 communication. The PLC program was done with TIA v11. Unfortunately the CPU was crushed. But, i have the back-up program. I upgrade the program into TIA v13 and Download to CPU 1214C Part# 214-1AG31-0XB0 & connect to existing TP700 Comfort.. At this point the PLC & HMI are communicating properly. I download that program into CPU1214C Part # 214-1AG40-0xb0 & connect toTP700 Comfort, The HMI give alarm that the recipee can not be written to PLC. But in the accessible Devices the PLC & TP700 is Reachable. Please help me... ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/23/2015 4:19:52 PMNew subject after splitting |
|
| 10/2/2015 3:51 PM | |
|
Posts: 8946 Rating:
|
214-1AG40 Check that FW version in HW-konfiguration is correct. |
Follow us on