11/29/2015 9:38 AM | |
Posts: 1 Rating:
|
Hi, We have a problem on our 6SN1118-0AA11-0AA0 card. there is an "ERROR CODE 2" displayed on the card and we don't know what the error means. Badly need help on how to eliminate this error. What are the things needs to be done? Thank you very much in advance.... ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/30/2015 10:26:52 AMNew subject after splitting |
|
12/2/2015 3:36 AM | |
Joined: 10/17/2007 Last visit: 7/14/2024 Posts: 4008 Rating:
|
Error "2" is "rotor position" problem. that is the one installed on the motor end (non shaft end)--it working together with control card. possible the cable connecting it NG, or connector on the 6SN1118- card(15 pin D type) loose, cable shield grounding NG ? or the cable defective. normally this component is not likely defective itself. HTH
|
If you like my comments please |
|
Follow us on