12/17/2015 12:35 AM | |
Joined: 11/4/2013 Last visit: 3/11/2022 Posts: 1 Rating: (0) |
s7 1200 PID basic continuous/ 7 basic v12sp1 Is it possible to set the output LOWER limit at a positive value? The configuration window works well to set the UPPER limit but I cannot set a positive lower output limit.
Example: output upper limit 40% and lower limit 20%. I have cascading loops and a want to limit the range of the reference used by the subsequent loop. This easily done in s7 v5.4 sp3.1 but I cannot do it in 7 basic v12sp1 ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/17/2015 2:49:18 PMNew subject after splitting Last edited by: James Fox at: 12/20/2015 5:00:28 AM |
|
Follow us on