1/23/2016 8:30 PM | |
Joined: 11/29/2011 Last visit: 4/29/2024 Posts: 1354 Rating: (229) |
Hi,
"S7-1200, S7-300, S7-400 and ET 200S CPU as I-Device support up to two Application Relations (AR), S7-1500 as I-Device a maximum of four ARs." |
- What you read here, please check with manuals and your requirements. |
|
1/24/2016 2:48 PM | |
Posts: 5 Rating: (0) |
For the I-Device the only limit is the maximum process image. Be careful for the update timer on the network.
|
1/25/2016 7:44 AM | |
Joined: 5/12/2006 Last visit: 4/30/2024 Posts: 22243 Rating: (2981)
|
Hello, first you should check if you S7-400 support the I-Device Feature. Look in this list: Then if you will assign the i-Device to more then one controller yoiú must use the Regards |
This contribution was helpful to1 thankful Users |
1/25/2016 8:03 AM | |
Posts: 5 Rating: (0) |
The I-Device is shared with maximum 2 PLC. However with one PLC you can read some difference I-Device, depending of the I/O image |
Follow us on