2/11/2016 2:11 PM | |
Joined: 12/18/2014 Last visit: 7/26/2024 Posts: 33420 Rating: (4147) |
Here is a simple example of using the PI controller. The input I1 is switched between manual and automatic mode of the controller. The setpoint can be changed via the display. AttachmentPI-controller.zip (243 Downloads) |
This contribution was helpful to1 thankful Users |
2/11/2016 2:47 PM | |
Posts: 17 Rating: (0) |
Thank you ixo. I'll take a look but it will certainly help. |
2/11/2016 6:32 PM | |
Joined: 12/18/2014 Last visit: 7/26/2024 Posts: 33420 Rating: (4147) |
A small example of the power on / off with a hysteresis range. The threshold values can be set via the display.
AttachmentON_OFF.zip (218 Downloads) |
2/12/2016 10:26 AM | |
Posts: 17 Rating: (0) |
But first i just want to replace the sensor and make an on/off system to see if it works. Tank you |
2/24/2016 8:48 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
New question published by Le Test !! is split to a separate thread with the subject Best Ultrasonic sensor for a tank of water. Best regards |
2/24/2016 1:50 PM | |
Joined: 8/5/2015 Last visit: 9/20/2021 Posts: 120 Rating: (6) |
here you are program for example
AttachmentCircuit Diagram1.zip (222 Downloads) |
Follow us on