2/12/2016 3:01 PM | |
Posts: 1 Rating:
|
hi i have PCS7 wincc V6.0...i am facing two problems. 1. after power failure one of client 's project not opening and message is "The configured server is not available". i still have project backup but that only one client not loading this project and other 7 clients working normal. when i restart this client pc ,it is not auto starting wincc explorer...then i start manually wincc it gives some error ...i am attaching this error image. 2. i prepare other pc as a client and install wincc and sql server 2000 , security patch of xp....but i need help for configuration of client that i can connect it with server in place of faulty client. if user manual available it will help thanks ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/15/2016 2:43:54 PMNew subject after splitting |
|
Follow us on