2/15/2016 7:02 PM | |
Joined: 8/27/2014 Last visit: 9/9/2022 Posts: 10 Rating: (0) |
I have a problem with the FB45 function. I need to recompile it but i can't because i don't have de password. Where can I find the FB45 compiled function for S7-1500?? ------------------------------------------------------------------------------------------ |
Last edited by: mihaiTC at: 2/15/2016 7:03:43 PMLast edited by: Min_Moderator at: 2/16/2016 10:37:48 AMNew subject after splitting |
|
2/16/2016 10:58 AM | |
Joined: 5/12/2006 Last visit: 7/25/2024 Posts: 22324 Rating: (2999)
|
Hello, here you can download the SCL Source File . https://support.industry.siemens.com/cs/de/en/view/109476945 or here? https://support.industry.siemens.com/cs/de/en/view/90063944 Regards Christoph |
Last edited by: ChristophD at: 2/16/2016 10:59:42 AM |
|
2/18/2016 10:45 AM | |
Joined: 10/1/2013 Last visit: 5/8/2024 Posts: 605 Rating: (71) |
Well, those blocks are not the FB45 but ChristophD is right, you should use the ident profile or the ident blocks to work with RFID and S7-1500. When using TIA Portal V13 SP1 or greater those blocks are already included in TIA Portal at "Instructions" > "Optinal packages" > "SIMATIC Ident". |
Follow us on