2/23/2016 2:07 AM | |
Joined: 7/15/2007 Last visit: 7/3/2024 Posts: 54 Rating: (0) |
Good evening, I need to use the PDM software 8.x with Tia Portal V13sp1 Update7 and need to know if integrated on the platform and if ocaciona problem? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/23/2016 1:06:44 PMNew subject after splitting |
|
2/24/2016 9:53 PM | |
Joined: 3/14/2008 Last visit: 10/8/2024 Posts: 2109 Rating: (941) |
Good evening Nelson, I checked PDM software (v8.0, v8.1 and 9.0), but it shows no entries with TIA portal. Attached is a screenshot of the compatibility of PDM 9.0, which not differs from previous versions. Only Step7 software and PCS7 is compatible. In the compatibility tool from Siemens I cannot select Simatic PDM, which indicates it's not working with TIA portal. In the future, if you need to know if two software programs work together, you can use the Compatibility tool. It's a very handy tool where you select one software program/package and check which other software works together with no issues. Check the following link: https://support.industry.siemens.com/kompatool/pages/main/index.jsf?sitc=wwdfi10002 Hope I've helped you.... |
Last edited by: Oreca at: 2/24/2016 9:54:11 PMLast edited by: Oreca at: 2/24/2016 10:13:21 PMLast edited by: Oreca at: 2/24/2016 10:13:52 PMIf I could help you, you can use the RATE button. Thank you. |
|
2/24/2016 11:38 PM | |
Joined: 9/27/2006 Last visit: 10/10/2024 Posts: 12286 Rating: (2685) |
Hello Nelson; In the case,of PDM software Oreca's good advice might cause a little confusion. You will find in the Compatibility Tool no mention of PDM with TIA Portal, while PDM is described as compatible with Step 7 and PCS 7. But that is only for the requirement of PDM Integration in Step 7 (Simatic Manager) or PCS 7. I have used PDM with non-Siemens Profibus masters in the past, which requires you must get a PDM license as Stand-Alone; it will work the same with TIA Portal (until Siemens decides to provide integration packages). Simatic Manager (for PDM) will be installed on your programming computer so you can configure your instruments with PDM over Profibus-DP or Profinet (to PA or HART). You should have a look at this Application Example that shows an installation of PDM 8.0 with TIA Portal v13; whatever network you choose to use (this example is for HART instruments) the requirements would be similar: How do you incorporate HART field devices with SIMATIC PDM in the TIA Portal? https://support.industry.siemens.com/cs/ww/en/view/109478959 Attached you will find a table of the types of licenses you can get for PDM (taken form the Siemens Industry Mall). Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 2/25/2016 12:18:02 AM |
|
2/25/2016 7:00 AM | |
Joined: 3/14/2008 Last visit: 10/8/2024 Posts: 2109 Rating: (941) |
Hi Daniel, I've read that Simatic PDM was also available as standalone component, but it was not mentioned in any of the documents, only Step7/PCS7. So in that case, it's indeed confusing. For the record, I wrote a feedback on the tool. Maybe Siemens can incorporate this in a next version of the compatibility tool. |
Last edited by: Oreca at: 2/25/2016 7:07:17 AMLast edited by: Oreca at: 2/25/2016 7:15:41 AMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
3/1/2016 7:09 AM | |
Joined: 3/14/2008 Last visit: 10/8/2024 Posts: 2109 Rating: (941) |
So, I asked about the missing standalone PDM package. I thought I'd share it with you guys:
Many thanks for your sent request. Please excuse, that we can only send you our answer today.
Here our answer.
Theme compatibility.
The STEP 7 classic product SIMATIC PDM V8.2 SP1 is compatible with STEP 7 V5.5 SP4 and PCS7 V8.1.
The installation of SIMATIC PDM V8.2 SP1 and STEP 7 (TIA Portal) V13 SP1 must be possible. The software can be installed but the user doesn`t get any warning.
Also, a side by side utilization must be work. Please always follow the released MS Windows operating system for the respective products.
Another statement to the "compatibility" between the products SIMATIC PDM V8.2 SP1 and STEP 7 (TIA Portal) V13 SP1 is not currently us.
Theme Compatibility Tool.
Your comment:
"Because SIMATIC PDM standalone cannot be selected in the Compatibility tool."
Our answer:
Currently there are no plans the product SIMATIC PDM as a main product in the Compatibility tool to integrate. Possibly that is still realized in the future.
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on