3/1/2016 11:24 PM | |
Posts: 3 Rating: (0) |
hello everyone!! recently I've updated my TIA family to v13 SP1.I heard that S7-1200 simulation had some repairs in last version but there is no difference.....I can't get online or download my program to virtual device(simulation). at first I open PLC SIM and create a new project for S7-1200 then I compile my hardware with no problem. in ''extended download to device'' window as you see in the following picture,I had a compatible device in target subnet.after selecting that device and pressing load button,the ''load result'' windows appears as shown in the picture and I have an error while loading and downloading.I don't know where the problem is. I should say that I test the same action with S7-1500 and the other families without any problem. in my control panel, the ''set pc/pg interface'' access point of the application is ''PLCSIM S71200/S7-1500'' and assigned as ''PLCSIM S71200/S7-1500.TCPIP.1'' who can tell me the proper steps for getting online or downloading?where is the problem? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/2/2016 9:35:38 AMNew subject after splitting |
|
3/1/2016 11:45 PM | |
Posts: 3 Rating: (0) |
thank you so much.....I found my problem in getting online.that's all because of the version of CPU !!! |
This contribution was helpful to1 thankful Users |
Follow us on