3/16/2016 11:18 PM | |
Joined: 1/22/2016 Last visit: 10/30/2024 Posts: 3 Rating: (0) |
It is being realized retrofit of a machine, which already updated the NCU and we are updating the HMI in which it replaced one MMC103 by a PCU 50.5 - C, for the upgrade are working with the software versions mentioned above and we find these problems, we can not view the data in the appropriate screens to timer, counters and program selection. Attached photos and project files
In the help HMI pro was to revised data bar of DB59, to activate the corresponding DB counters , timer and type of selection to display its contents and there are no results, we have exhausted all possible options for viewing data in cells, and we believe that this missing some initial configuration or some more structured problem to be solved otherwise
More information: •With which Project-DVD do you work ( version and identification )? HMIpro RT 7.3.0.22 Toolobox 6.5 Librery TL2000_V733_uk
•For which customer is the machine? ThyssenKrupp Metalúrgica De México, S.A. de C.V.
•HMI PRO Textproject This file is the folder: 1.rar
•Step7 Project This file is the folder: Giusti_4.rar
• The version on HMI PRO CS V07.03.00.35
Attached photos:
Photograph 285: Counter photography
Photograph 286: Timer photography also you can see an error in TAKTZEITEN.FROM_LAND: 1031
Photograph 287: Type selection screen photography ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/17/2016 2:16:16 PMNew subject after splitting |
|
3/16/2016 11:19 PM | |
Joined: 1/22/2016 Last visit: 10/30/2024 Posts: 3 Rating: (0) |
286 |
Follow us on