3/24/2016 11:30 PM | |
Posts: 2 Rating: (0) |
Hi, guys, I have the same problem SMF had. LLD file displayed a java error, upon copying a rung. I deleted the rung, then I saved the program. When I tried to open it again, the progress bar filled to 100%, then got frozen. If I try to open the file from the LOGO!soft, the status bar repeatedly fills to 100% (few dozen times). I tried to open the file with a V7 LOGO!soft, but didn't work. Can you help me repair the file? Many thanks! ------------------------------------------------------------------------------------------ AttachmentConveyor bad file.zip (233 Downloads) |
Last edited by: Min_Moderator at: 3/29/2016 1:55:55 PMNew subject after splitting |
|
Follow us on